The construction of CERALOCK is shown as below, and ceramic element is hold as a two durability beams. This element is a ceramic thin plate (<100μm), so that it may caused a crack in ceramic element (this crack will lead to no oscillation) when strong external stress is added.
Metal cap is fixed on the substrate by adhesive. So when strong external force is added to the metal cap, it may come off.
Please do not handle with a strong external force to the ceramic resonator (both body and metal cap).
Note:Structure drawings are provided on our website "my Murata".
"my Murata" requires registration for access, and can be found through the following link. (Entry is Free)
We hope that the utilization of is advantageous so we may innovate together !