Select your region & language

CES 2026

CES 2026

Powered By Innovation: Showcasing Intelligent System Technologies for Mobility, Wellness, and Connectivity at CES 2026

Murata will join other industry leaders at CES 2026 January 6-9 in Las Vegas at West Hall's Booth 4399 (Vehicle Technology & Advanced Mobility Pavilion). Our solution experts will be on hand to spotlight how intelligent systems and precision sensing are reshaping the way we live, move, and connect. Potential and existing customers, partners, and fellow innovators will see an extensive line-up of product demos and technologies, as well as those still under development* including:

smart mobility

Smart Mobility: Mobility is evolving - and so is our ability to navigate it. Murata's MEMS-based systems, GNSS-free positioning, and sensor-enabled platforms are paving the way for safer, smarter movement.

Embedded RFID Tire Tag and Sensing

Enhance road safety and sustainability with real-time visibility into tire condition and age with our tire-embedded RFID tags, offering a compact, durable design that ensures consistent performance in all driving conditions.

 

Gyro Compass

Find true north in less than one minute with Murata’s new Gyro Compass. The fast and relatively inexpensive solution will enhance autonomous cars but will also make it possible to navigate and position accurately in completely new applications.

Headlight Leveling Using MEMS

Enable headlight leveling at a lower cost and reduced weight by replacing traditional suspension sensors and wire harnesses with an IMU and fusion algorithm.

 

Motion Tracing Using Low Frequency Magnetic Fields

Achieve accurate position detection and tracking with our Low Frequency Rx and Tx antenna coils. The magnetic field link is resistant to environmental interference such as the human body or surrounding structures for a robust and precise tracking system.

High-Precision Positioning and Headlight Leveling

(In Conjunction with Hexagon)

Experience headlight leveling using MEMS and safety-certified positioning in real-time for autonomous driving, V2X, advanced navigation and ADAS applications. Hexagon and Murata are shaping the future of autonomy with reliable, precise positioning and sensor technology. In-vehicle demos can be scheduled here.

embedded connectivity

Embedded Connectivity: With advanced Wi-Fi®, Bluetooth®, and Ultra-Wideband (UWB) modules, we’re building the embedded backbone of intelligent infrastructure – delivering precise location detection and coverage across vast areas.

Wi-Fi® Mesh for Range Extension

Expand Wi Fi® coverage to enhance more robust wireless networks across construction, agriculture, heavy equipment, and AGV/AMR operations. Dynamic routing mesh technology delivers dependable machine to machine connectivity in challenging environments.

Wi-Fi® HaLow (Type 2HK/Type 2HL Module)

Solve IoT connectivity gaps with our sub 1GHz Type 2HK Wi Fi® HaLow module, delivering up to 1 km coverage and over 1 Mbps for industrial, smart metering, smart building, and camera IoT devices.

Type 2NR Module

Overcome miniaturization and integration constraints without compromising performance or design flexibility with our Type 2NR module. Based on the Nordic nRF54L15 SoC, this module offers feature rich designs for IoT devices in a small form factor.

Indoor Location Tracking with Bluetooth® Channel Sounding

Deliver high precision asset tracking using Bluetooth® Channel Sounding and our proprietary algorithm, enabling a single anchor device to determine the tag’s position for streamlined location tracking.

Satellite Position Tracking

Report the location information of various assets in real-time using both terrestrial and non terrestrial networks with our connectivity modules, ensuring accurate, reliable global positioning and tracking in any environment.

Wonder Stone

Wonder Stone uses Murata’s 3D Haptics to guide users with vibrations, light, and sound. It mimics push/pull sensations, syncs with heartbeats, and shifts colors with temperature and mood – enabling navigation, even for the visually impaired.

UWB Smart Lock

Enable safe, convenient, touch-free entry with smart door locks and smartphones using our ultra-small, high-precision Ultra-Wideband (UWB) connectivity modules.

health-centric sensing

Health-Centric Sensing: From molecular analysis to wearable biosensors, Murata’s technologies are redefining how health is monitored – non-invasively, continuously, and intelligently.

Molecular Analysis Platform 1, 2

Analyze DNA/RNA targets in 15 minutes anywhere, without a lab. Our compact, universal platform pairs disposable cassettes with a mobile app, using AI-powered diagnostics to protect people, food, water, and the environment.

Vios Monitoring System

Vios Medical creates smart tools for continuous patient monitoring, delivering hospital-grade cardiac telemetry, vital signs tracking, and 24/7 remote ECG surveillance to enable timely intervention and support recovery.

Smart Ring Enabled by Picoleaf™

Deliver precise, multifunctional performance in smart wearables with the Multi-Layer LCP rigid flex board and Picoleaf™ sensor technology. Together they fit advanced circuits, antennas, and responsive user interfaces into the compact, curved form of a smart ring.

Mask Voice Clip

A mask-mounted voice input device that isolates the speaker’s voice in noisy environments. This next-gen interface enhances human-tech interaction, redefining communication and improving clarity in challenging acoustic settings.

ultrasonic tech

Ultrasonic Tech: Ultrasound isn’t just for imaging – it’s powering cleaning, tracking, and sensing in ways never imagined.

Ultrasonic Cleaning Device

Enhance driving safety in any weather with our ultrasonic cleaning device, removing water and debris from camera lenses. Our advanced parking sensors improve short range visibility, helping drivers maneuver with confidence.

Ultrasonic Tracking Powered by pMUT

Murata’s ultrasonic tracking solution combines advanced pMUT sensor technology with Sensoryx’s precise algorithms to deliver accurate 3D spatial and position tracking (6DOF). Ideal for XR ; it offers low power, compact design, and robust performance.

Airborne Ultrasound Transmission Metamaterial

Transmit ultrasound through plastic and metal with metamaterial arrays, enabling bi-directional communication and enhancing the performance of ultrasound sensing and communication systems.

other solutions

Other Solutions

Vibration Sensor

Delivering precise, reliable detection of acceleration and oscillations in demanding environments. Featuring high sensitivity, low noise, and robust design, Murata’s vibration sensor enables predictive maintenance, improved safety, and optimized performance in industrial and automotive systems.

CO₂ Sensor

Offering compact, low power, and highly accurate gas concentration measurement for indoor air quality monitoring, HVAC systems, and smart devices, Murata’s CO2 sensor enables energy efficiency, healthier environments, and regulatory compliance.


 

To set a time to meet with Murata during CES 2026, please visit here.

 

  • *At the time of this announcement, some of the exhibit products are concept products or under development. Specifications and appearance are subject to change without notice.

  • 1. This product has not been approved by the U.S. Food and Drug Administration (FDA).
  • 2. Murata’s products as incorporated into this platform are not considered medical devices.

About Murata

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter
PageTOP