Select your region & language

Murata High Output FORTELION Battery Module Equipped with Lithium-Ion Secondary Battery

  • Batteries

8/6/2020


Murata Manufacturing Co., Ltd.
President:
Norio Nakajima

Murata Manufacturing Co., Ltd. has developed the MH1701, a FORTELION high-output battery module that is ideal for industrial equipment requiring high output such as uninterruptible power supply (UPS) devices and instantaneous voltage drop compensators, and plans to begin mass production in August. This module is equipped with “FORTELION,” Murata’s proprietary lithium-ion secondary battery, which uses olivine-type lithium iron phosphate as the cathode material and combines long life with an exceptionally high level of safety.

In recent years, in keeping with the progress of IoT (the Internet of Things), the use of electronic control devices has grown and a more stable power supply is required than before at data centers and factories where precision equipment is manufactured. Accordingly, operators of such facilities have expanded their use of UPS and Ancillary Service in the interests of ensuring stable power supplies in the event of power outages. Conventionally, these devices are equipped with lead-acid batteries, but in view of issues such as short battery life, there is an increasing need to replace them with lithium-ion secondary batteries which feature longer battery life as well as space-saving and weight-saving capabilities.

In response to these needs, Murata has developed this high output battery module that features FORTELION’s sophisticated input-output characteristics, a high level of safety, and longer battery life.

Highlights

  • Safe storage batteries
    Thanks to the stable crystalline structure made possible by employing olivine-type lithium iron phosphate as the cathode material, FORTELION is less vulnerable to breakage and less likely to catch fire, even if subjected to a large impact or significant pressure, and maintains a reliable battery performance even under intense workloads.
    FORTELION has received the Japanese safety standard for the emergency power systems “Emergency Power Supply Certification” and has its safety has been recognized in a test report based on the UL9540A international safety standard for storage battery fire risk in the US.
  • Longer life than conventional lead-acid or lithium-ion secondary batteries
    This product equipped with FORTELION is capable of undergoing 15,000 charge-discharge cycles. FORTELION provides a much longer expected operating life than lead-acid batteries that typically require replacement after around 500 cycles or regular lithium-ion secondary batteries that are capable of 2,000 to 3,000 cycles, thereby contributing to reducing LCC (life cycle cost).
  • Continuous discharge at up to 200A (6C)
    The optimized secondary battery module structure and circuit design make possible continuous discharge from SOC 100% to 0% at 200A. This allows a greater power output than the previous product,*1 providing more appropriate solutions for short-time backup use or instantaneous voltage drop protection systems.
*1 Compared with Murata’s previous model IJ1201M

Major Applications

  • UPS (uninterruptible power supply)
  • Instantaneous voltage drop compensators
  • Ancillary services (short-period frequency regulation) *2
*2 Special operational services to maintain the quality of electricity

Summary of Specifications

Product name MH1701
Rating capacity 1.75kWh
Nominal voltage 51.2V
Maximum discharge current 200A
Maximum charge current 100A
Operating ambient temperature -20°C to +50°C
Dimensions W435×H80×D570mm
Weight 26kg

Murata will continue to develop secondary batteries and modules to meet the market’s needs and contribute to realizing a safe, secure, natural disaster-resistant sustainable society through these technologies and solutions.

Visit FORTELION MH1701 High Output Battery Module for more details.

Related website

International Standard “UL9540A” Report Which Examines Fire Risk Due to Battery Cells Obtained for First Time in Japan~ Contributing to the Construction of Safe Energy Storage Systems in U.S. Metropolitan Area Buildings ~

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter