Select your region & language

Ceramic Capacitors FAQQIs it safe to use multilayer ceramic capacitors in excess of the rated voltage condition?

A
Do not apply a voltage to the capacitor that exceeds the rated voltage as called out in the specifications.
Applied voltage between the terminals of a capacitor shall be less than or equal to the rated voltage.

  1. When AC voltage is superimposed on DC voltage, the zero-to-peak voltage shall not exceed the rated DC voltage.
    When AC voltage or pulse voltage is applied, the peak-to-peak voltage shall not exceed the rated DC voltage.
  2. Abnormal voltages (surge voltage, static electricity, pulse voltage, etc.) shall not exceed the rated DC voltage.
Swipe left or right to change screens View in landscape mode
Is it safe to use multilayer ceramic capacitors in excess of the rated voltage condition?