Select your region & language

Silicon Capacitors FAQQPlease explain how to read the part numbers.

A

The part number of a silicon capacitor consists of 15 alphanumeric characters.
Characters 1 to 6 are the series name; 7 and 8 indicate the BDV; 9 indicates the size; 10 to 12 indicate the capacitance value; 13 and 14 indicate the packing configuration; and the 15th character indicates the electrode surface material.
Pay particular attention to the way the capacitance value is indicated, as this differs from that used for MLCC products.
Refer to the information below for details on how to read part numbers.

Related terms : Silicon Capacitor (Si-Cap), Silicon IPD (Si-IPD, Integrated Passive Device), Size Code, Part number (PN), part number assignment rules