Select your region & language

LoRa FAQQWhat is the realistic range of LoRa? What is the actual range that can be achieved?

A

The stated range is more than 10 km, between 15 to 20 km. We would say typically 10 km. However, there are other factors that will influence this "realistic range" - such as, the network and node-gateway positioning, surrounding environment (presence of physical obstacles), antenna performance, Tx power mode, etc.

Additional remarks: Our team has done an actual trial indoor, and we were able to transmit as far as 7km without any issue. (*7km was the maximum indoor area at that point of time) Hence, in actual, the reach would have been much further.

Return to LoRa Module Page

Back to LoRa FAQ List