Select your region & language

Power Products FAQ QWhat will happen if the external capacitor is larger than the maximum capacitance value?

A

The inrush current at startup may become large. That may cause the overcurrent protection circuit to activate and lead to a startup failure.
Please design and use the system so that the capacitor is equal to or less than the maximum capacitance value.