Select your region & language

CO2 sensor FAQ QHow do these sensors compensate for temperature effects and atmospheric pressure fluctuations?

A

The impact of the temperature on the CO2 concentration is compensated for using the built-in sensor. There is a 0.14%/hPa atmospheric pressure dependency. Please compensate for the impact in your calculations according to the compensation formula listed on the datasheet.