Select your region & language

Soil sensor FAQQMy measurements (temperature, volumetric water content, EC) seem too high (or too low).

A

Refer to the recommended installation information and confirm that the product is installed properly.
If readings are abnormal even after confirming that the product has been installed properly, please contact us using the inquiry form.