Select your region & language

NTC Thermistors FAQQ[NC* Series] Why isn't the B constant a negative value?

A

See B constant in the Basic Knowledge . From the thermistor characteristic equation, the resistance value is proportional to the B constant and the temperature 1/T. If the horizontal axis is 1/T, the graph has a positive slope. The B constant is therefore a positive value.