Digital Panel Meters FAQQHow is the half-digit displayed?

A
The half-digit, or left-most '1', is always OFF (not visible) with display readings between "000" and "999" on 3½ digit meters and between "0000" and "9999" on 4½ digit meters. The half-digit is turned ON with display readings greater than or equal to "1000" on 3½ digit meters and with display readings greater than or equal to "10000" on 4½ digit meters. An enabled half-digit in combination with all other digits OFF is used to indicate an input overrange condition which occurs when the applied input exceeds the meter's measurement capability.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。