LoRa FAQQWhy should I choose LoRa? Is LoRa(WAN) better than other technologies?

A

It is clear that LoRa is de facto dominant in a few (mainly European for now) markets in the public IoT network space. LoRaWAN has the benefit of being an alliance with an Open approach instead of a proprietary one. There are also technological differences between the various solutions.

However, the main question is and remains: What goals do you want to achieve with your IoT project?

No technology is perfect. The openness of LoRa is a benefit compared with the proprietary approach of Sigfox but, along with its reliance on unlicense spectrum this openness is also a problem.

There is never a one-size-fits-all solution. It is rarely about 'this' versus 'that' technology. In most cases it is about 'which mix of technologies will make me reach my IoT projects goals?'.

*Extracted from: LoRa and LoRaWAN: the technologies, ecosystems, use cases and marketOpen in New Window

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。