LoRa FAQQHow many LoRa nodes can be connected to one gateway? Is mesh topology possible in LoRa?

A

It depends on the gateway specifications which is usually defined by the number of packets it can support. 

For instance, if there is a 8-channel Gateway supporting 1.5M packets/day, and if the application sends 1 packet per hour, then more than 62,000 nodes can be handled by that Gateway.

Theoretically, mesh topology is possible. However, LoRa is defined for star-topology only.

Return to LoRa Module Page

Back to LoRa FAQ List

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。