Digital Panel Meters FAQ

Topic: 2-Wi2re Meter

What happens when a 2-wire meter's input signal polarity is reversed?

Absolutely nothing - the display will not operate. Except for ac-mains powered devices whose inputs are not polarity sensitive, all DATEL 2-wire meters are fully protected against reversed-polarity inputs (i.e., "input signals that are hooked up backwards").
请配合完成FAQ改善问卷。
FAQ对您有帮助吗?
如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。
※以这一方式提出的疑问及要求将不予以回复。 发送
如您有产品相关的疑问,请点击“联系我们”进行咨询。