Digital Panel Meters FAQQCan I remove the built-in CTs on your ac ammeters and then reconnect them remotely?

A
Our ac ammeters retain their UL-recognized component status when used in their factory-supplied configuration. Any modifications made to these ammeters voids their UL certification, including remotely mounting the built-in CTs, removing the terminal blocks, or any modification that involves disassembly of the ammeter or its components.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。