Although this product is applicable to UN38.3, it conforms to the Special Provision 188, therefore it can be shipped as an exemption from Class 9 dangerous goods.
However, in air transportation, it is necessary to be transported as Class 9 dangerous goods in accordance with IATA DGR (Dangerous Goods Regulation) and Packing Instruction 965-Section IB. In addition, when the number of package is not more than one as per single consignment, it can be shipped in accordance with Packing Instruction 965-Section Ⅱ.
The above regulation is effective only for the packing condition at the time of shipment from the Murata factory. If any problem happens under the packing condition other than Murata specification, Murata would not have any responsibility for the compensation. For the details of transportation regulation, please refer to the latest edition of IATA DGR (Dangerous Goods Regulation), IMO IMDG Code.