Ceramic Capacitors FAQQPlease provide data regarding the frequency characteristics in the event that the measurement conditions (ambient temperature and the applied voltage of the direct current) of the multilayer ceramic capacitors are changed. (Ex: Frequency characteristic data at 40℃ and 3VDC)

A
Data regarding the temperature characteristics and DC bias characteristics, AC voltage characteristics, impedance/ESR and other frequency characteristics, ripple exothermic characteristics and other major electrical characteristics of multilayer ceramic capacitors can be verified in the "Simsurfing" design support tool.
Data for changed measurement conditions and graphs comparing multiple part numbers can also be displayed. In addition, you can download data on each of the electrical characteristics in CSV and other formats and data sheets showing the electrical characteristics in PDF format (data sheets that present data for the major electrical characteristics of each product on one page). For more details, refer to "How to use Simsurfing".

Related FAQ

> What is the allowable Ripple current Murata's ceramic capacitors can withstand?
> What are the typical ESR values of multilayer ceramic capacitors?
> What is the reason that the nominal capacitance value cannot be obtained?
> The capacitance-frequency characteristics displayed by SimSurfing differ from the nominal capacitance. What is the reason for this?


Related Links

> Design Support Tool FAQ
> Design Support Software SimSurfing

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.