AParts are automotive tested and approved. Classification has been done according to CISPR22 class B requirements. The results are on the level of 20dBuV/m with the bandwidth of 100kHz - 1GHz. Our customers have not indicated any EMI problems so far.