Select your region & language

Inclinometers FAQQWhat is the difference between an accelerometer and an inclinometer?

A
Murata Electronics Oy's inclinometers and accelerometers are all based on the same MEMS capacitive measuring technology. Different product versions are optimized for different purposes, determined by the g-range in which they are going to be used. The maximum g-range of the inclinometers is earth's gravitation (approximately 1g) . Murata Electronics Oy's accelerometers measure low-g ranges of ±0.26g up to ±12 g.