Select your region & language

Inclinometers FAQQIs it also possible to get inclinometers with linearity error of no more than 0.5mg in ±0.1g measurement range and what is linearity change as a function of temperature (if any) ?

A
Yes, please ask the measuring results of linearity from Murata. Results are from between ±30 degree. For example in ± 0.1g measuring range the linearity is better than 0.5mg.