Select your region & language

Inclinometers FAQQMurata Electronics Oy has mentioned, that SCA61T and SCA100 have 8Hz frequency response with 0.002° resolution of analog output and in datasheets the frequency response of both of them is said to be 8...28Hz. What is the difference?

A
The SCA 61T and SCA100T are similar regarding the original frequency response. The frequency response in the Data-Sheet (8...28 Hz) describes the max variation of the -3dB point between individual parts and it is the same for the both of the sensor types.