Ceramic Capacitors FAQQAre there ceramic capacitors that can be used to replace film capacitors?

A

The key feature of film capacitors is that changes in temperature or voltage do not cause much change in the capacitance.
The capacitance of temperature compensation type ceramic capacitors (MLCCs and lead type capacitors) also does not exhibit much change from changes in temperature or voltage.
When replacing a film capacitor with a Murata ceramic capacitor, verify the specifications in the film capacitor description (series, capacitance, voltage, etc.) to choose a matching capacitor from our temperature compensation type ceramic capacitor lineup.
For the contents of the performance warranty, see the detailed specifications sheetDetailed specifications sheet
.

Please ensure there are no issues with your device before use.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.