Select your region & language

Ceramic Capacitors FAQQWhat are the differences between the GQM, GJM, and GRM series?

A

A major difference between the GQM, GJM, and GRM series is in the capacitor composition. (See Figure 1)
For the GJM and GQM series, the difference lies in the rated voltage. For the GRM series, nickel (Ni) is used as the inner electrode material, whereas low-resistance copper (Cu) is used for the GQM and GJM series. The use of low-resistance copper allows for a low equivalent series resistance (ESR) to be achieved in the capacitor.
This low ESR, in turn, results in a high Q (hi-Q) in GQM and GJM series capacitors, making them ideal for temperature compensation types in circuits operating at high frequencies, including VHF, UHF, and microwave bands.

Series GQM Series GJM Series GRM Series
Rated voltage >100Vdc ≦100Vdc N/A
Inner electrode Copper (Cu) Copper (Cu) Nickel (Ni)
Applications High frequency circuits High frequency circuits -

<Figure 1>

<Related Links>
GRM Series
GJM Series
GQM Series