Select your region & language

Piezoelectric Diaphragms FAQQWhat is the recommended procedure when soldering the lead wires on a Piezoelectric Diaphragm.

A
■Soldering Condition with iron
Pre-heating (60 to 80°C, 10 sec. min)

Component Part Temperature (°C) Time (sec. max.)
Electrode 320 to 350 0.5
Metal Plate 410 to 450 3.0
Diaphragm

■ Position
The farthest position from the center of the Piezoelectric Diaphragm is recommended, because the soldering point works as a load that restricts its oscillation. 
The lead wire should also be as fine as possible. (Ex: AWG32).

Related FAQs
Most people who viewed this page also referred to the following pages.
Q. Are there any points to be aware of handling diaphragm with lead wires?