Select your region & language

Digital Panel Meters FAQQHow is the half-digit displayed?

A
The half-digit, or left-most '1', is always OFF (not visible) with display readings between "000" and "999" on 3½ digit meters and between "0000" and "9999" on 4½ digit meters. The half-digit is turned ON with display readings greater than or equal to "1000" on 3½ digit meters and with display readings greater than or equal to "10000" on 4½ digit meters. An enabled half-digit in combination with all other digits OFF is used to indicate an input overrange condition which occurs when the applied input exceeds the meter's measurement capability.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.