Select your region & language

Ceramic Resonators (CERALOCK) FAQQWhy does frequency correlation occur when CERALOCK is mounted in opposite direction?

A
CERALOCK have two built-in load capacitors inside, CL1 at input side and  CL2 at  output side. Capacitance value of CL1 and CL2 are not completely equal.

Oscillation frequency : Fosc is approximated by following formula.
When CERALOCK is mounted in opposite side, positions of built-in load capacitors CL1 and CL2 are switched. Because of the difference of capacitance value of CL1 and CL2, frequency correlation occur.

Approximation Formula of FoscCircuit

Related FAQs
Most people who viewed this page also referred to the following pages.
Q.
Is there any problem if CERALOCK is mounted in opposite direction?
Q.
Does CERALOCK have orientation?
Q.
What are the meanings of the Marking?