Murata Manufacturing Co., Ltd. (hereinafter “Murata”) has commercialized the LQP02HQ_Z2 series RF inductors for in-vehicle communication devices (hereinafter “this product”). Despite its small, 01005 inch size, this product features quality performance that accommodates strict requirements, including the AEC-Q200*1 qualification for the automotive industry. Mass production began in March 2025.
The automotive industry is seeing continuous evolution in sensing and communication functions in recent years due to the proliferation of autonomous driving technologies. Along with the full-scale expansion of 5G service, V2X*2 is attracting notable attention. Using the existing LQP02HQ_02 series for consumer devices as the base, Murata achieved High-Q characteristics by applying the inductance control technique which was developed based on feedback from the connectivity module development site. This new product has the reliability required for automotive infotainment and comfort devices. As a result, it enables stable signal transmission, contributing to robust connectivity in automobiles and base stations.
Check the LQP02HQ_Z2 series for product details.
For information on RF inductors for in-vehicle applications, click here.
To request a free small-quantity sample (20 pcs) of this product, click here
For inquiries on this product, click here
Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.