Select your region & language

Inclinometers FAQQIs the analog output capable of higher resolution than the SPI interface?

A
Yes, the resolution of the analog output is higher than the digital one. The analog resolution is limited by the output noise density of SCA61T. The noise is 15 µg/√Hz and it yields the following resolutions: 0 - 0.1Hz=>resolution 5 µg, 0 -1 Hz=> resolution 15 µg, 0 - 10 Hz=>resolution = 50 µg, 0 - 30Hz=>resolution is 80 µg

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.