Murata to exhibit at IDF 2016

Intel Developer Forum 2016

8/18/2016

We're pleased to announce that Murata Electronics will be exhibiting at the Intel Developer Forum August 16–18, 2016.

Moscone Center West, San Francisco, CA
Come visit Murata at Booth 322 

Technology Showcase Exhibition Hours:
Tuesday, August 16 11:00 am–7:00 pm
Wednesday, August 17 11:00 am–1:00 pm / 4:00 pm–7:00 pm
Thursday, August 18 11:00 am–2:00 pm

See how Murata is shaping the future of optical engines for high-speed network computing, IoT, and Wearables.

Murata products and demos featured at IDF:

Fiber Optical Transceivers

  • Murata will feature 20Gbps/ch x 2ch x bi-direction, small size optical engine matched with the Thunderbolt3 interface. Murata’s optical module can be installed by SMD reflow assembly process. Optical coupling is done easily using a simple pluggable connector.
  • 10Gbps/ch, 14Gbps/ch, and 25Gbps/ch FOT modules will also be exhibited. 

Wireless Optical Transceiver

  • New technology to achieve 10Gbps near field communication.
  • DEMO (Murata collaboration with Intel)

µDC-DC converter

  • Murata will display a small case size, low EMI noise µDC-DC converter module that integrates a power inductor in the ferrite multilayer substrate. We will also exhibit aPoint-of-Load module for system boards.

Crystal

  • Murata’s advanced package technology allows for balanced competitive performance and cost.

Wireless Connectivity Modules

Sensors:

  • Piezo vibe (Haptics motor using piezo element) DEMO
  • Pressure sensor (Capacitive air pressure sensor) DEMO
  • Heart Rate sensor (Small HR sensor with green LED) DEMO

For more information visit www.murata.com.
If you would like to meet with Murata during IDF, contact Anthony Fung.
We look forward to seeing you at IDF 16.


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com