Low Profile 2.0 mm Max./470 μF Capacitance Polymer Capacitor Commercialized

  • Capacitor

6/16/2023


Murata Manufacturing Co., Ltd. (hereinafter “Murata”) has developed a polymer aluminum electrolytic smoothing capacitor that achieves Murata’s largest capacitance (470 μF) in a D case (7.3 x 4.3 mm) with a maximum product height of 2.0 mm. Mass production of this capacitor will begin in June 2023.

In recent years, the high-speed processing of increasingly larger volumes of data has been necessary at data centers. With this necessity, there is an increasing trend toward the implementation of not only high-performance networks and accelerators but also faster servers, which are the core equipment at data centers. However, this equipment consumes a large amount of current, and there are two issues that must be managed for stable operation: IC voltage fluctuation and IC heat generation. To solve these issues, it is necessary to both increase the capacitance of the capacitors used to suppress voltage fluctuations and to mount large, high-performance heat sinks (cooling units) on the ICs. Because conventional high-profile and high-capacitance capacitors placed near the IC would hit the heat sink, multiple low-profile yet low-capacitance capacitors are now arranged in a row for higher capacitance.

It is with this that Murata developed a low-profile, high-capacitance, and low-ESR polymer capacitor that does not hit the heat sinks and also helps lower the number of components required. This capacitor not only reduces the amount of surface area required for mounting on electronic components, but also helps lower component costs.
In addition, the miniaturization of the products allows for reductions in the materials used and energy consumption during processing, helping to reduce the products’ environmental impact.

Specifications

左右にスワイプ可能です 横持ちでご覧ください
Product name ECASD40E477M006KA0
Size (L x W x T) 7.3×4.3×1.9mm(T2.0mmMax)
Rated voltage 2.5Vdc
Capacitance 470μF±20%
ESR 6mΩ

Product pages

Go here for details on the "ECAS" series

Inquiries

Go here for inquiries on the "ECAS" series

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter