Select your region & language

Murata’s New Multi-Protocol Wireless Module Enables Simultaneous Use of Wi-Fi 6 and Matter

  • Connectivity Modules

3/16/2023

Murata Manufacturing Co., Ltd.
President:
Norio Nakajima

Exploring new opportunities in wireless communication, leading electronics manufacturer Murata introduces its latest engineering innovations at Embedded World 2023, Nuremberg. (14th - 16th March. Hall 4A Stand 4A-645)

Featuring the company’s proprietary expertise, the new LBES5PL2EL module is highly optimized to meet the exacting demands of next generation IoT hardware - where having MatterTM connectivity is set to become an increasingly important expectation. This module is based on a highly-integrated IW612 single-chip 2.4/5GHz solution from NXP, which covers a broad array of different wireless protocols. Through this, 1x1 dual-band Wi-FiTM (IEEE 802.11a/b/g/n/ac/ax), Bluetooth® 5.3 and IEEE 802.15.4 are all incorporated into the Murata tri-radio module.

Inclusion of LE Audio functionality is another important plus point, especially in relation to voice-controlled products. This latest generation of Bluetooth technology delivers heightened performance, while drawing less power, and is predicted to replace many of the current BR/EDR Bluetooth-based audio connections in the near future.

Also being made available is the LBEE5PL2DL module. This is based on the NXP IW611 device and features both Wi-Fi 6 and Bluetooth 5.3 support.

Among the intended applications for these newly announced modules will be home automation equipment, digital assistants, smart domestic appliances, lighting gateways, climate control systems and EV charging points. FCC/IC and TELEC certification plus conductive tests for CE are all available, thereby helping customers using these modules to accelerate their time to market and keep product development costs down.

The Murata LBES5PL2EL and LBEE5PL2DL wireless combo modules are each supplied in compact surface-mount packages, with dimensions of just 8.8mm x 7.7mm x 1.3mm. For more information on LBES5PL2EL go to: LINKS
(For more information on LBEE5PL2DL please visit contact form.)

“There are still only a few Matter-compliant solutions on the market, yet the potential for it to deliver convenience and comfort to the places in which we live is huge,” states Akira Sasaki, Director of the Communication Module Division at Murata. “Thanks to the introduction of the LBES5PL2EL, we are now able to provide full support for Matter, including Thread, alongside Wi-Fi 6. This will be a real value to engineers developing hardware for home/building automation, as well as for numerous other purposes.”

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter