Select your region & language

Murata’s Combined LC type EMI Suppression Filters have High Attenuation Characteristics for Modern Devices

  • Noise Suppression Products / EMI Suppression Filters / TVS Diodes (ESD Protection Devices)

1/21/2015

Murata Manufacturing Co., Ltd.
President/Statutory Representative Director:
Tsuneo Murata

Murata announced the launch of its BNX series of surface mount, LC combined-type EMI suppression filters for the automotive, industrial electronic equipment, and healthcare markets.  The filters employ an exclusive circuit configuration combining capacitors and ferrite beads to achieve superior frequency characteristics and excellent attenuation characteristics for highly effective noise damping.
In recent years, the trend toward more sophisticated functionality in set devices has intensified the need to reduce noise levels and this has driven the demand for noise filters with improved attenuation characteristics.  In response to this market demand, Murata has developed the BNX026/27/28/29 series of EMI suppression filters that deliver high attenuation characteristics over a wider bandwidth range. 

The new series of DC line noise filters cover a wide range of frequencies, from the kilohertz to the gigahertz bands. The filters are also compatible with large currents and high voltages, making them suitable for a broad range of applications. 

Insertion loss characteristics enable high attenuation rates of 35dB or more over a wide range from 15kHz to 1GHz.  BNX filters with a current rating of 15A are ideal for power supply circuits susceptible to low-frequency-band noise, whilst parts with a voltage rating of 50V (BNX026H01 and BNX027H01) are suitable for automotive applications requiring support for high voltages. 

Murata’s BNX series of EMI filters are suitable for noise reduction on DC power lines in electronic equipment, automobiles, medical equipment, factory automation equipment, control equipment, communication equipment, digital AV equipment, and other applications.  Mass production is currently underway at plants in Japan.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter