Select your region & language

Murata releases common mode choke coil for in-vehicle SerDes PoC Interface

  • Noise Suppression Products / EMI Suppression Filters / TVS Diodes (ESD Protection Devices)

5/31/2021

Murata manufacturing Co., Ltd has released the latest automotive common mode choke coils, DLW21SH391XQ2 and DLW21PH201XQ2 used to suppress noise for high-speed interfaces that use Serializer/Deserializer (Ser/Des)*1 on Power Over Coax (PoC)*2. Mass production started in May.

In recent years, various sensors (vehicle-mounted cameras, LiDAR*3, radars, etc.) are equipped to vehicles to establish self-driving car technologies. Since SerDes is often used on image data transmission interfaces, this has led to the application of PoC which performs data and power transmission on single coaxial cables in order to reduce the amount of cables. Since a large current flows through compared to conventional differential interfaces (several tens of mA currents), we have developed these products which are capable of withstanding large currents such as 300 mA and 500 mA.

Today, more detection sensors (cameras, LIDAR, radar, etc…) are being integrated into today’s self-driving automobiles. SerDes is often used in image data transmission interfaces, that has led to the application of using PoC, which combines data and power transmission over a single coaxial line to reduce the amount of cable.

Since this technology requires higher current compared to conventional differential interfaces (typically tens of mA), the latest Murata DLW21 products are designed to handle 300mA to 500mA.
Since each sensor is compact, it is difficult to increase GND*4 patterns on PCB, and noise issues may occur. By inserting these 2012 size (2.0 × 1.2 mm/0805 inch) products between the data transmission line and the GND line, you can expect noise suppression effects even with their compact size.

Product information pages

Glossary

  • *1SerDes (Serializer/Deserializer): Circuits that convert between the serial and parallel signals in each direction.
  • *2PoC (Power Over Coax): A method that combines the signal line and power line to a single coaxial cable.
  • *3LiDAR (Light Detection and Ranging): A system that detects obstacles around the vehicle by emitting lasers.
  • *4GND (Ground): Circuit that returns currents that have gone through the signal line and power line. Common mode noise may occur more frequently if the GND impedance cannot be reduced sufficiently.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter