Select your region & language

Murata announces chip ferrite beads with highest ever current capabilities

  • Noise Suppression Products / EMI Suppression Filters / TVS Diodes (ESD Protection Devices)

8/2/2022

Murata Manufacturing Co., Ltd.
President:
Norio Nakajima

Murata has introduced the BLE32SN series of chip ferrite beads. These are the world’s first chip-type noise suppression components to have 20A current rating. They will be used to provide noise suppression in circuits with large current flows, such as the battery charging systems and powertrains of electric vehicles (EVs), as well as in industrial equipment.

There was previously no chip-type noise suppression filter that could attain a 20A current rating. This meant that multiple chips had to be mounted in parallel, which added to the bill-of-materials (BoM) costs and took up valuable board real estate. Through specifying Murata’s BLE32SN series, a small number of chips will be required* - enabling space savings and weight reductions to be realized within implementations.

  • *When compared to using standard 10A-rated noise suppression chips.

By leveraging advanced structural simulation techniques, Murata engineers have been successful in creating a proprietary internal electrode design. This increases the electrode volume of these chips compared with those using a conventional arrangement. It has resulted in a significant lowering of their DC resistance characteristics. Consequently, heat generation is reduced, so less thermal management is needed - allowing further cost and weight savings to be benefitted from.

Murata’s BLE32SN series ferrite beads have a compact form factor, with 3.2mm × 2.5mm × 2mm dimensions. They are capable of supporting an operational temperature range of −55°C to +125°C or −55°C to +150°C, depending on customers’ application requirements.

Product pages

For more information, please visit product details site.

Inquiries

Please contact us for details: contact form

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter