Murata Manufacturing Co., Ltd. (hereinafter "Murata") has added a new DLW32SH510XF2 (hereinafter "this product") lineup that meets DCMR*2 Class 3*3 requirements to the automotive use chip common mode choke coil DLW32SH_XF Series for next-generation CAN FD*1 in-vehicle networking applications. Mass production of this product began in April 2023.
In the automotive industry in recent years, the aim to make driving safer and easier has been driving the rapid development in the sophistication of vehicle control technology through the implementation of technologies such as ADAS (Advanced Driver Assistance Systems). This trend has led to a rise in the demand for faster in-vehicle networks and an increased switch from Classical CAN*4, which had a maximum data rate of 1 Mbps (bits per second), to the faster CAN FD. In response to this demand, Murata has expanded the lineup of CAN FD-compatible chip common mode choke coils to include new 51µH products with existing 100µH products. This product is effective in reducing noise from CAN or CAN-FD signal lines in in-vehicle networks.
Satisfies DCMR Class 3 requirements for common mode choke coils used in CAN FD networks as specified in IEC62228-3*5
For product details, see DLW32SH510XF2.
For the series lineup, see DLW32SH_XF2.
Murata publishes a list of common mode chokes recommended for each application.
See here for a list of products for signal lines for in-vehicle applications.
For inquiries on this product, see here.
Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.