Select your region & language

Highest L value added to 0804mm inductors LQW04AN_10 series

  • Inductors

9/28/2015

Highest L value added to 0804mm inductors LQW04AN_10 series

Background

Murata has now released the LQW04AN_10 series of high-frequency winding-type inductors in the 0804 mm size. The scope of inductance values is 36 to 56 nH, providing a lineup of higher inductance values than the existing LQW04AN_00 series (1.1 to 33 nH). With the 0804 mm winding inductance value, we have achieved the industry’s largest inductance value of 56 nH.
Going forward, we will enhance our lineup in this series with inductors having higher Q characteristics than our conventional products in the field of inductance up to 36 nH.
  

Features

The industry’s largest inductance value (56 nH) in the 0804 mm size
  

Parts List

LQW04AN_10 Series
See here for the series lineup.
See here for the spec sheet (including precautions, mounting information and packaging).
 

Production

Mass Production


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter