Select your region & language

01005 high frequency chip inductors with superior Q characteristics from Murata

  • Inductors

1/25/2016

Murata Manufacturing Co., Ltd.
President/Statutory Representative Director:
Tsuneo Murata

Overview

Murata Manufacturing Co., Ltd. today announced the market launch of its LQP02HQ series of film-type high-frequency chip inductors in the ultra-compact 01005 size (0.4 x 0.2 mm).

Background

Along with the trend toward increased multiband capability, multi-functionality and ever more sophisticated functions, the configuration of the RF circuits in smartphones and other compact mobile devices is becoming more complex, and the number of components being incorporated is increasing. At the same time, the volume accounted for by the batteries inside these mobile devices has become larger and larger, necessitating the RF circuits to be configured in more limited spaces. This is one reason for the rising demand for ultra-compact RF inductors with high Q*1 characteristics capable of reducing circuit loss to the absolute minimum.

It is against this backdrop that Murata has developed and released the LQP02HQ series of inductors whose Q characteristics are further improved over those of the company’s LQP02TQ series. Using the company’s latest proprietary microprocessing technology, these products feature the optimum coil patterns and L-shaped electrode construction. By enlarging the dimension in the height direction rather than in the horizontal direction, Murata has achieved the world’s highest Q characteristics in the 01005 size. These characteristics are on a par with those of its LQP03TN_02 series in the 0201 size. 

Another feature is that, thanks to the use of high-accuracy monolithic processing technology, the new components support an inductor tolerance of ±0.05 nH (0.4 to 1.5 nH), which is the world’s lowest.

The series lineup consists of 57 items with inductance values that range from 0.4 nH to 22 nH, and Murata will be continuing its efforts to further increase the inductance values of its future components while also developing even smaller components with high Q characteristics.
The LQP02HQ series does not contain any materials whose use is restricted by the RoHS Directive.*2

*1: Q = This is the reciprocal of the dielectric dissipation factor (DF). The higher the Q value, the lower the loss and also the more efficient the inductor.
*2: RoHS Directive = The Restriction of Hazardous Substances Directive restricts the use of lead, cadmium, mercury, hexavalent chromium, PBB, and PBDE in electrical and electronic devices. 

Features

  • Ultra-compact 01005 size (0.4 x 0.2 x 0.3 mm)
  • World’s highest Q characteristics achieved in the 01005 size
  • Ultra-tight tolerance (inductance tolerance: ±0.05 nH [0.4 to 1.5 nH]) that is the world’s lowest in the 01005 size
  • Product line consisting of 57 items (with inductance values ranging from 0.4 nH to 22 nH)

Applications

  • High-frequency modules (PA/ANT/SAW/GPS, etc.) for cell phones
  • Smartphones, cell phones (WCDMA/GSM/LTE, etc.)
  • Wi-Fi/Bluetooth® and other wireless module types
  • All types of high-frequency circuits

Part number

For further details of the LQP02HQ series lineup, click here.

Electric characteristics

Comparison between a product in the new series (LQP02HQ3N9B02) with a previously available product (LQP03TN3N9B02)

Comparison between a product in the new series (LQP02HQ2N2B02) with a previously available product (LQP03TN2N2B02)

Q characteristics of selected items

 

External size

 

Production

Mass production began in January 2016 at the Miyazaki Plant of Fukui Murata Manufacturing Co., Ltd.

Sample price

¥5/piece

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter