Select your region & language

Power inductors for 5G offer improvements in Isat and RDC specifications

  • Inductors

12/2/2021

Murata Manufacturing Co., Ltd.
President:
Norio Nakajima

Murata announces availability of the DFE21CCN_EL series of power inductors for 5G smartphones. Intended for use in DC/DC converters and power management circuitry, these components signify major enhancements in operational performance parameters when compared to the company’s conventional inductors. They exhibit a 20% increase in saturation current (Isat) and a 50% reduction in DC resistance (RDC) over their predecessors. These parameters help to raise operational efficiency levels and enable downsizing of system designs.

The new Murata inductors make use of the company’s long-established expertise in materials science – with specially developed metal materials and an optimized molding technique. The innovative L-shaped electrodes allow these components to reach considerably higher density levels than those from other manufacturers.

The DFE21CCNR24MEL has a 0.24 µH inductance value, with an RDC of 20mOhm (Max) and an Isat of 6.5A (Max). For the DFE21CCNR47MEL, the key values are 0.47 µH for inductance, 29mOhm (Max) for RDC and 4.8 A (Max) for Isat. The 1.0 µH-rated DFE21CCN1R0MEL and 2.2 µH-rated DFE21CCN2R2MEL have respective typical RDC figures of 60mOhm and 138mOhm, with Isat figures of 3.3A and 2.1A. Murata’s DFE21CCN_EL series components are supplied in 0805 inch size format. See the data sheet for additional details.

“Under normal circumstances, if you look to improve the Isat value of a power inductor, then its RDC will suffer accordingly,” explains Tomohiro Yao, EMI Division, General Manager of Marketing & Promotion Department, at Murata. “Thanks to the technological advances we have been able to implement, from both process and structural perspectives, we have succeeded in improving Isat and RDC simultaneously, with no necessary trade-offs.”

For more information about the product, please visit: product details site.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter