New Murata DC-DC Converters Optimized for GaN Gate Drive Applications

  • Power Products

11/24/2022

Murata Manufacturing Co., Ltd.
President:
Norio Nakajima

Leveraging proprietary PCB electrical and mechanical design topologies, Murata has introduced a new series of compact DC-DC converters that are aligned with the increasing prevalence of wide bandgap technology. The new MGN1 series of 1W output DC-DC converters are designed to deliver the voltages needed by the gate drivers of GaN devices.

These units provide low-profile, small footprint, surface-mount solutions that can be easily integrated into space-limited systems. They also have the advantage of being lightweight, which opens up even greater deployment opportunities. The output voltages offered are +8V, +12V and +6/-3V.

One of the key attributes of MGN1 series DC-DC converters is their ultra-low isolation capacitance of 2.5pF (typical). Through this, the coupling of transients across the isolation barrier is minimized, thereby preventing signal distortion. In addition, it means that system EMI problems can be mitigated. The >200kV/µs common mode transient immunity (CMTI) of these units makes them well suited to the elevated switching speeds of GaN-based systems, further ensuring gate driver signal integrity. Thanks to their partial discharge performance, reliable operation is maintained in high voltage conditions.

The DC-DC converters in Murata’s MGN1 series support a continuous isolation barrier withstand voltage of 1.1kV, with UL62368 conformance pending for 650VDC basic insulation and 240VAC reinforced insulation. These converters have 6.5mm creepage and clearance figures. A -40°C to +105°C working temperature range allows them to be installed into extremely challenging environments. In addition, reverse polarity and short circuit protection mechanisms are both incorporated.

There are a wide range of GaN-based applications that the new DC-DC converters can be used for. These include EV fast charging infrastructure, battery storage converters, smart grid implementations, solar inverters, solid-state switching breakers, ICT and data centre, wind turbines and motor drives.

Inquiries

Please contact us for details: contact form

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter