Select your region & language

Expanding the NTC thermistor lineup: compact sizes with high-precision temperature sensing for mobile, consumer, and medical devices

  • Thermistors (Temperature Sensors, Current Control)

3/19/2025

Murata Manufacturing Co., Ltd. (hereinafter "Murata") expands its lineup of SMD-type NTC thermistors, specifically the "NCP Series," which offers high-precision temperature measurement across the entire operating temperature range. The new additions include the 0402M and 0603M sizes, specifically designed for mobile, consumer, and medical devices. Mass production has already begun for these products, and samples can also be provided.

As electronic devices such as smartphones and wearable devices acquire advanced performance with higher component densities, the load on electronic components is increasing, generating more heat. In recent years, however, as the performance of equipped ICs has improved and the number of mounted electronic components has increased, the importance of thermal designs is becoming more critical by the day. Under such circumstances, the demand for high-precision temperature sensing has significantly increased to ensure efficient application performance. Taking advantage of Murata's years of processing technology development, these compact products are capable of achieving high precision temperature sensing.
Murata will continue to expand its product lineup to meet market demand.

Features

  • Capable of high precision temperature sensing in all temperature ranges, achieving ±0.1°C at 25°C (refer to the following graph)
  • Because these products have the same characteristics as our existing products (1005M size), there is no need to change the design, contributing to increasing their component density as well as saving space on the circuit board
  • Since it has a smaller volume compared to the existing model (1005M size), this new model is capable of fast response (the 0603M size has approximately 80% smaller volume and 70% less mounting area. The 0402M size has approximately 90% smaller volume and approximately 80% less mounting area.)

Temperature sensing accuracy

The red lines in the graph indicate the temperature sensing accuracy of Product D, which has been newly added to the lineup.


  • F and D in the graph indicate the resistance tolerance from the part number configuration. Here, the black line indicates Product F and the red line Product D.

Specifications

Product number NCP02WF104D05RH NCP03WF104D05RL
Applications Mobile device Consumer device, medical device [GHTF A/B]
Size 0.4 x 0.2 x 0.2 mm 0.6 x 0.3 x 0.3 mm
Resistance (25°C) 100 kohm±0.5% 100 kohm±0.5%
Constant B (25/50°C) 4250 K±0.5% 4250 K±0.5%

Product pages

Inquiries

  • For inquiries on these products, see here.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter