Murata Manufacturing Co., Ltd. has recently released the XRCGB-F-S series for Wi-Fi devices. The 2.0 × 1.6 mm size high-precision crystal units are in mass production with samples available.
These products achieve an initial frequency accuracy of +/−10 ppm in the 37.4, 38.4, and 40 MHz frequency bands and an operating temperature range of −40 to +105°C. This means the components can withstand high temperatures and are ideal for applications such as lighting fixtures, HEMS/BEMS, or devices equipped with wireless functionality such as Bluetooth™ Low Energy, or Zigbee®.
Devices equipped with Wi-Fi or Bluetooth™ functionality
Wireless modules, headsets, over-the-top (OTT), game devices, wearables, lighting fixtures, HEMS/BEMS, etc.
Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com