Ceramic Capacitors FAQQWhat kind of Ceramic Capacitors do you have?

A

Ceramic capacitors are categorized by the shape, structure, and material / characteristics of the dielectric ceramics, as follows.


<Category by dielectric ceramics>

  Temperature Compensating Type
High Dielectric Type
Main Temperature Characteristics
C0G, U2J characteristics, etc.
X5R, X7R characteristics, etc.
Dielectric ceramics
Paraelectric titanium oxide (TiO2) or calcium zirconate (CaZrO3), etc.
Ferroelectric barium titanate (BaTiO3), etc.
Features
The characteristics of this material are that the relative dielectric constant changes almost linearly with the temperature. The change in the capacitance value over time is negligible. Even in high temperatures, high voltages, and high frequencies, the tanδ (loss of capacitor) remains low and is excellent in stability.
Since this material provides a high relative dielectric constant from 1,000 - 20,000 at room temperature, small sizes and large capacity can be acquired.

Related link

What is the difference in the features and applications between the high dielectric type (X5R/B, X7R/R etc.) and the temperature compensating type (CH, C0G, etc.)?


<Category by shape and structure>

  Structure Examples of shapes
SMD

Multilayer
Resin molding
 (Disc type)
SMD2
Lead type Multilayer
Disc type

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.