A proprietary film developed by Murata is used as the dielectric in the FH Series. The material is a thermosetting resin with a high dielectric constant, which makes film capacitors with high heat resistance and compact size possible. Furthermore, unlike heat-resistant PET products, FH Series capacitors have a self-healing function that operates even in the high-temperature range, contributing to their high reliability.