Select your region & language

Digital Panel Meters FAQQCan I use a combination of one ACA5-20PC ammeter, a 3-position selector switch, and three 5A CTs to monitor current in a 3-phase ac circuit?

A
Yes, but the selector switch must be a special type referred to as a “make-before-break” switch specifically designed for this type of application. A CT’s secondary output-winding can generate extremely high—and potentially lethal—voltages when the current flowing in its output leads is suddenly interrupted by disconnecting the CT’s output from the ACA5-20PC. Electro Switch Corporation’s www.electroswitch.com part number ‘2409C’ control switch is specifically recommended for this type of application.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.