Slight differences in the inductor characteristics may affect the RF performance
in RF circuits mainly using LQG and LQP. Inductors do not have polarity. However, their structure is
not completely symmetrical. Therefore, differences arise in the characteristics due to the mounting
direction. Accordingly, we give markings to ensure that these components are mounted in a unified
direction. We do not have a component direction we recommend. Therefore, please consider the
component placement upon confirming the difference in impact depending on the inductor direction.
Related links
Please refer to here
for the impact the mounting direction has on the characteristics.