Select your region & language

LoRa FAQQWe are defining the antenna for our prototypes. Does the RF pin already have the matching components to have 50 ohm impedance, or we need to add it externally?

A

Please refer to my Murata.
We have the detailed information on the schematics, etc. The Pin is 50 ohms, but, there can be antenna tuning network which customer might implement. There is also reference antenna information that customer should use.

Return to LoRa Module Page

Back to LoRa FAQ List

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.