Select your region & language

Power Products FAQ QThe MYBSP series isolated DC-DC converters for PoE do not start when under no load or light load conditions.

A

They do not start because they do not satisfy the MPS (Maintain Power Signature) requirements.
Use the following method to set the consumption current of the PSE output so that it exceeds 10mA at all times.

  • Have it consume power at the PSE output
  • Add a dummy resistor, etc. to the DC-DC converter output to have it consume power

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.