Enter a product part number, or a portion of a part number.
There are two types of ceramic capacitors: the high dielectric type and the temperature-compensating type. They have different circuit application uses, so be sure to understand the differences in terms of characteristics before use.
Example [Temperature characteristics]
Example [DC bias characteristics]
As ceramic capacitors for temperature compensation have no DC bias characteristic, there is no change in capacitance.
<Reference FAQ> Does the capacitance change when a DC voltage is applied to ceramic capacitors? Are there any points to be aware of regarding changes in the capacitance? Please tell us whether the capacitance of the ceramic capacitors changes with time. Also, please tell us about any points to pay attention to regarding time-dependent changes.
<Related Links> Design Support Software SimSurfing
We appreciate your cooperation with the FAQ improvement questionnaire.Were these FAQs helpful?
We would like to hear your opinions and requests regarding these FAQs.Opinions from customers will be used to improve the FAQs.We will not respond to inquiries and requests received by this form.
For product inquiries, please contact us using our contact form.