From , search for products using one of the following search methods.
On the search results page, select the checkbox for the products you want to compare, and then press the Compare button (up to five part numbers can be selected).
The currently selected part numbers are remembered even if you leave the page. For example, you can compare two parts, A and B, by first searching for part number A and selecting it for comparison, and then searching for part number B and selecting it for comparison. Press the "Selected part numbers" button if you want to view or remove your selections.
If there is no electrical characteristic data associated with a part number, no checkbox appears and it cannot be selected.
The comparison graph results page shows the status, part numbers, and features of each part, indicating any differences in red. When you unselect a checkbox, it hides the graphs.
When you hover the cursor over the graph lines, the corresponding values are displayed. You can also print the graphs or download the values in CSV format.
You can press the "Setting details" button to change the type of graph or configure the axes.
For example, if you change the frequency characteristic lZl to Q on the graph and press the "Set using this content" button, the graph changes as follows.