Ultrasonic Sensors FAQ

Characteristics
Waterproof type/Open-Structure type/High-Frequency type

Do the ultrasonic waves interfere with remote control communication using 40kHz waves?
Do they interfere only with sound waves?

Ultrasonic waves have no impact on electromagnetic waves. Note, however, that, if the 40kHz signal line runs in close vicinity of the ultrasonic sensor, noise from the signal line could be superimposed on the sensor signal, reducing the S/N ratio. Since the recipient sensor signal line has a high impedance, it is recommended that it be connected in the shortest possible length and shielded to minimize the impact of crosstalk and external noise. 

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.